So attractive — magnetic charging cables from Goobay

Apple’s Macbook has had a convenient magnetic connector for the charging cable for years. This not only prevents unnecessary fumbling when trying to insert it, but it is also a life saver when it comes to (cable) accidents. If you stumble over this cable, it just falls out of the port without knocking the whole computer off the table. With the magnetic charging cables from Goobay, this technology is now also available for Android smartphones.

From Micro USB to magnet clip — no scratching or fumbling

The vast majority of Android smartphones and tablets have the same port for the charging cable and data transfer: Micro USB. Goobay offers a suitable adapter with magnetic connector for the 1.2 metre-long charging cable.

The adapter is simply inserted into the Micro USB port where protrudes about a millimetre from the device. Ideally, the adapter should stay in the device at all times thereby preventing dust build-up, scratches and wear from the daily inserting and removing of the charging cable.

The Goobay charging cable automatically connects with the magnetic connector and then only needs to be placed near the smartphone. Unlike with the Micro USB, the charging cable can no longer be inserted the wrong way around. It is perfect for convenient, quick and reliable charging of smartphones and the application is considerably more convenient than conventional charging via Micro USB.

Simply magnetic — The Goobay adapter

The magnetic adapter from Goobay is the convenient alternative for charging via Micro USB. Smartphones and tablets can be easily connected to power supplies or laptops without hassle. And thanks to the universal adapter, it now works on all Micro-USB-enabled devices.

Image source: www.reichelt.de

Leave a Reply

Your email address will not be published. Required fields are marked *